This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4513-SP: Common mode filter capacitor

Part Number: THS4513-SP


The THS4513-SP recommends 0.2uF capacitor for the CM pin.

We have a situation where an op-amp is driving the CM voltage but it cannot drive 0.2uF. A series 50 ohm buffer resistor could be used to isolate the amplifier from the capacitive load but that would require an expensive layout / rework.

Would 0.02uF of capacitance be acceptable for the common-mode bypass capacitor for the THS4513-SP? What degradation might be seen?