This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR105: Vcm MIN

Part Number: XTR105

Good morning,

I used XTR105 with RTD, piezo bridge and potentiometer without problems.

In the new application I connected a humity sensor (Homeywell HIH-4000-001) to the Vin inputs of XTR105, the prototipe works OK.

I checked again the values and I found the Vin+ signal start from 0.67V(RH 0%) to 3.24V (RH 100%), Vin- is fixed to 0.67V, all respect Iret pin.

I've always thought that the Vin+ and Vin- must be 1.25V greater than Iret voltage, like datasheet specification.

Where am I wrong?

Thanks

Davide