Other Parts Discussed in Thread: THS3491, THS3217, THS3091, LM7372
Hi I'm seeing a long slow settling time tail for this part when used as a differential amplifier with x5 gain 500Ohm feedback and 100 Ohm input resistors. power pins are well decoupled and have less than 10mV of change so it's not a power supply rejection ratio issue. Resistors are metal foil 0.2ppm/C temperature coefficient so super stable. I did consider it being input bias drift with temperature but it's too fast for that and the bias drift would be less than10% of this amount based on power dissipation and coefficient shown on the datasheet. Settling time is quoted as 40nS to 0.1% for +/-15V supply unity gain on the datasheet. I'm seeing 200nS to 0.2% for x5 gain Is this an expected part characteristic or can you think why this is so slow ? Thanks Steve