Part Number: LM675
Other Parts Discussed in Thread: TPS55340, OPA548
Hi Experts,
I have built and tested a circuit with LM675 to generate voltage pulses by using an adder circuit. The pedestal level is 24V and above that pulses go about 6V. The circuit is working successfully. The nominal load is 0.5A.
Now, I wanted to add output short circuit protection to the LM675 incase the output PULS_OUT+ gets shorted to ground and current tries to go above 0.5A. Hence, I added a circuit as shown page 1 of attached circuit. Page 2 shows the 24V and from that 34V output generated using TPS55340.
When I tested the circuit by shorting the output to PULS_OUT+ to ground, the load current becomes zero and the 34V drops to around 8V. However, even after removing the short circuit, the 34V remains around 8V. If I switch OFF the circuit and switch ON, it works as normal. My intention is that in ON condition, if a short circuit occurs, the output path should become open and upon removal or short circuit, the circuit should return to its normal working.
Any suggestion what would be missing in this peice of circuit and how to overcome that?LM375 Short Circuit Protection.pdf