Other Parts Discussed in Thread: LM317, OPA2677, THS3491
To whom it may concern,
I would like a recommendation of an opamp product that can provide 500mA peak current and is stable under capacitive load of 300pF.
Basically, the load is a current source that can pull a peak current of 500mA in parallel with an equivalent capacitor of 300pF.
The bandwidth should be around 60MHz.
Typically opamp requires a series damping resistor at the output (like OPA2674) for large capacitive load, but if the load needs to pull continuous current at the same time, this series resistor would create a large voltage drop.
I wonder if there is a product that can drive capacitive load and provide high output current at the same time, without a series resistor.
Thank you.
Weiyu