Other Parts Discussed in Thread: INA214
I am using a INA214 for a somewhat unique go/no go current detection system (essentially a current comparator) and I need to know the tolerance of the 10K ohm input resistance for the INA214.
Alternatively, I could work with knowing how closely balanced that the two input resistances are to each other.
I need to place large protective resistances in series with the inputs. Yes, I know the gain will be strongly affected, but since I really just need to detect current = yes or no above some threshold, then I know I can put the series resistors there as long as I account for some variability.
The data sheet tells me what is effectively the gain tolerance but that only sets the ratio, not the literal input resistance.
Thanks
Glen