Other Parts Discussed in Thread: LM311
Hi team,
I have to make an electronics project based on LM331, specifically an F-to-V converter, but I can only use the 5V power supply from the USB output of a common PC.
As I know, the USB output from a PC changes from 4.5V to 5.2V approximately, so I was thinking in a LDO of 4.2V for the Vcc of the LM331, do you think it is a good choice?
Because I don´t want to use a Boost converter beause of the noise...
PS: the input frequency range goes from 100Hz to 10KHz and it´s a square wave (0V - 3.3V) so I also have doubts about the choice of components.
PS2: the project statement doesn´t talk about LM331, I choose this because as I´ve read has a good features but any other suggestions for my conditions are very welcome.
Thanks.