This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2372-Q1: TLV2372 Multivibrator abnormal operation

Part Number: TLV2372-Q1

Dear TI community.

I have questions about multibrator behavior.

Multibrator was used for EV battery voltage measurements.
The attached file is a circuit diagram and a measurement waveform.

If only 12V low voltage is connected, it is normal to operate, but if HV (360V) battery is also connected, the waveform will change.

Please let me know if there are any considerations for the circuit or layout, or if there are any other solutions.Voltage sensing.pdf