This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP92064: is there a chip that supports SVID interface and SPI interface conversion?

Part Number: LMP92064


Hi

Hi, I see that Ti has a power chip that supports the SVID protocol. I would like to ask, can the SVID interface communicate directly with the SPI interface? If not, is there a chip that supports SVID interface and SPI interface conversion on TI?
Power monitoring chip LMP92064, SPI interface, but the size is a bit large, do you still have a smaller size, SPI interface power monitoring chip?