This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4513: Understanding Open loop gain with differential amplifier.

Part Number: THS4513

Hi

I am trying to test the Aol for THS4513. It is not behaving as expected.

With:

Vsupply:  ± 2.5v

     +Vin:     30mV

      -Vin:    -30mV

no feedback resistors.

I get  ~± .7v on the ouput; open loop gain of ~24.

Is this right? Where is the 63dB Aol coming from in the datasheet?

Also I currently do not have access to the Texas Instruments website or any of the app-notes or datasheets because my computers security software is malfunctioning. So I will not be able to open any link that is sent. 

Thanks

Tony