Other Parts Discussed in Thread: OPA192,
Hi team,
The customer used OPA2365 for PFC current sensing and the sensing resistor is 0.01Ω. Input voltage of the system is 200-264V and input current is 5.9A. The PFC and OPA192 schematic are as below. When unit did the 12ms cycle drop with full load(62.5A) at 264vac input, the PFC Mosfets Q103 or Q102 will damage. And OPA2365 output voltage was abnormal. Test waveform is as below. Do you have any idea why OPA2365 output voltage is abnormal under this situation?
Thanks very much.
best regards,
Sophia Yao