This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3201-Q1: I have a question to absolute maximum rating for TLV3201-Q1.

Part Number: TLV3201-Q1

Hi team,

I have a question about absolute maximum rating for TLV3201-Q1. 

This device has both of voltage and current range for input pins. Is it no issue when the current at input pin is less than 10mA even if the voltage at input pin is less than -10V?

Our customer uses resistor to limit input current less than 10mA. In this case, there is no impact even if the input voltage is out of maximum rating. Is it correct?

Regards,

Nishimura