This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2333-Q1:How to deal with the 1-way AMP PIN that OPA2333AQDRQ1 does not use?

Part Number: OPA2333-Q1


OPA2333AQDRQ1 One of the AMPs is not used. What should I do with the unused pins?

    The current processing is:

    5pin: pull down ground

    6pin, 7pin connected together

Is this okay? Any other suggestions?