Part Number: INA131
Hi. I need to know if there is some drawbacks trying to get an gain of about 1400 with the INA131, maybe instability or noise.
The amplifier is to be used with an input signal of 7 mV (load cell, 10 V, 350 ohms, INA131AP +/-15 V).
I need to adjust the output to 10 V with a single trimpot (Bourns 3296W 500 ohms) and adjusting the reference with an op amp (+/-2 V).
Thanks in advance.
Jose