Other Parts Discussed in Thread: OPA4376
When using OPA4376, we have the following problem:
using a single 5V power supply, applying about 2500 voltages to the non-inverting and inverting terminals, and the inverting terminal is 1mV or 2mV higher than the non-inverting terminal.
The op amp output voltage jumps around 160mV.
1. During static test, a fixed voltage of 2502mV and 2500mV is applied to the inverting terminal and the copper image terminal respectively, and the output result is a fixed value of 1mV (theoretical is 0mV), and the output is correct.
2. When we apply our signal source, the system transient, applying a voltage of about 2500 on the non-inverting and inverting terminals, the inverting terminal is 1mV or 2mV higher than the non-inverting terminal. The op amp output voltage jumps around 160mV. The output is incorrect.