Dear all,
I would like to ask a question about LMH6642.
If a short circuit occurs between the V (-) pin (No. 2 pin) and the + IN (No. 3 pin) pin, what phenomenon is considered to be caused by the cause?
As one of the conceivable cases, it can be assumed that a voltage exceeding −0.8 V is inputted to + IN when V− is 0 V (GND). Could you tell me if there is anything else?
Best Regards,
Y.Ottey