This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA193A-Q1: Volatge Output

Part Number: INA193A-Q1


Dear, Sir.

My customer is applying INA193A-Q1 for their system, now.

They use it under V+=5V, and Rs value is detemined to consider the

the peak of normal loading current level & Gain.

So, the peak of volatge output is closed to V+ -0.2V.

At this time, They are asking under over current for load situation such as

several times of the peak of normal loading current.

1. I think the output volatge will be clipped at V+ -0.2V during over current.

    I wonder my assumption is correct?

2. Is there no concern about the over current duration(clipping time) to consder

    the heating or anything alse?

Please give your advice.

Best Regards,

H. Sakai