This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM224: CMOS lower voltage version

Part Number: LM224
Other Parts Discussed in Thread: LM2904, LM258, OPA2170, TLV9102

I want to design a simple motion detection circuit with the mu Rata IRA-S210ST01 PIR.  The circuit shown on the datasheet would work just fine for me, but it requires the LM224 Op-Amp.  This runs at a different voltage than the PIR.  I would like my circuit to be battery operated, and operate between 5 - 12 vdc.  Is there another Op-Amp I can use in place of the LM224.  I really don't need a 14 pin package (4 op-amps).  Two (2) would suffice for my application.  Thank You.