Other Parts Discussed in Thread: THS3491, VCA820
Hi team,
My customer want to use this device as below, Vs=+/-5V, Vppmax=2V, frequency=30MHz, AVmax=40dB, we use the datasheet's equation,
Rg>385 ohm, Rf<19.2k, so we use these two value in this application. But when I use Vg=2V, Vpp=1mV, sine frequency=30MHz, I cannot get waveform in the output of the amp? Could you please share the reason?
- Can we use this device as above application?
- How to get the relationship between Vg and gain? When max gain is 40dB, I believe when Vg=2V, gain=40dB, when Vg=0V, gain=0dB. Right?