Hi,
Could you please tell me which value of the following "Figure 40" and "Table2" is correct regarding EMIRR IN+ ?
Best regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could you please tell me which value of the following "Figure 40" and "Table2" is correct regarding EMIRR IN+ ?
Best regards,
Kato
Kato-san,
The TLV2186 is a brand new product and the datasheet was just released. Unfortunately, it looks like an error in the EMIRR IN+ (dB) graph scale was made and not caught during review. The scale should start at 0 dB, and increase in +20 dB increments. If the vertical scale is viewed with the corrected values in place, then the Table 2 EMIRR IN+ numbers for the specified frequencies follow the curve.
I will let the engineer who is responsible for the datasheet know of the EMIRR IN+ graph issue. It is something we will need to correct. Thank you for bringing the issue to our attention.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Thomas-san,
Thank you for your quick response.
I understood and strongly hope that data sheet is revised.
Best regards,
Kato