Part Number: TLC27L2
Other Parts Discussed in Thread: TLC27L7
Hi,
What is the ESD Rating of TLC27L2? It is not in the specification.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Neal,
The HBM ESD rating is mentioned on pages 2 and 29.
The TLC27L2 and TLC27L7 incorporate internal ESD-protection circuits that prevent functional failures at
voltages up to 2000 V as tested under MIL-STD-883C, Method 3015.2; however, care should be exercised in
handling these devices as exposure to ESD may result in the degradation of the device parametric performance.