Other Parts Discussed in Thread: LMV331, TLV7032, TLV7042
VICR Common-mode input voltage range is only specified at 25°C
What is the performance for VICR Common-mode input over full operating temperature
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jesper
For devices with bipolar input stages such as the LMV331, VICR increases at temperatures above 25C and decreases at temperatures below 25C. Since the lmv331 can be operated down to -40C, it would be safe to assume that the VICR could shrink an additional 300mV as operation approaches -40C.
If your application requires a dual comparator with rail to rail input over temperature, I would recommend the TLV7042 (open-drain output) and TLV7032 (push pull output). These devices have CMOS input stages that allow the RRI capability.
Chuck
Jesper
I have not seen any follow up questions on this post, so I will close it out. If there is something else that we can assist on, please open a new request or reply to this one.
Thanks
Chuck