Dear colleague,
Our customer is planning to do a design in the brick power module for preventing current backflow. The previous solution is a diode, but as the power rate increases, a diode has more power dissipation. So we want to use this solution as the below picture. Why we need this function is because of tester special feature.
In normal mode, the tester provides DC voltage to the brick power module, max DC input is 200V.
In special mode, tester will act like short(K1 close), but at this moment, the energy storage capacitor has 200V voltage, if we don't prevent current backflow, it will happen short circuit and fail the test.
This may be a brick power industry standard, so if we could provide a solution, it will be significative.
So could you please reply to our 2 questions?
1. Whether the function is feasible?
2. How to calculate the detection speed? Customers want it as fast as possible.
Best Regards,
Rock Su