Part Number: INA3221
Dear TI Experts,
Could you kinldy provide the input capacitance of VIN+1/VIN-1;VIN+2/VIN-2;VIN+3/VIN-3 Pins? We can find it from datasheet, thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Bruce,
I am working on this now and will be back with an soon.
Sincerely,
Peter
Hey Bruce,
May I ask why this parameter is important for your design? Usually input capacitance is important when loading the inputs with resistors and this creating time constants for either the VBUS or VSHUNT signals; however, we don't recommend input resistors anyway as this will affect accuracy (section 8.4.3 of datasheet). I would not expect input capacitance to be greater than several pF, but I am still working on confirming this.
Best,
Peter
Hey Bruce,
Well if they are trying to measure 100MHz current, then they will want to pay attention to section 8.4.3 of datasheet. Current transients at harmonics of 500kHz can give the internal ADC problems. If they would want to measure average current they could use a RCR differential input filter to average the shunt voltage signal.
Best,
Peter