Other Parts Discussed in Thread: AMC1300, ISO1541, INA220, INA233
Dear Sirs:
My product needs to use current measurement in high voltage environment(ex:600V).
And I want to place INA226 in High Side to measure shunt resistor.(0.3mohm 1W 10pcs in parallel for 580A, and the error is limited under 1%)
But according to the INA226 SPEC, the common voltage restrict is 40 Volt.
Is there any problem to place an isolated OPA between INA226 and shunt resistor?
Do you have any suggested isolated OPA to match INA226?
Or other better solution for this case?
My percision still needs to be high like 16bits or 32bits.
Thanks~