Hello,
I would like to know how the noise spec was measured for this product. On the datasheet, it says that the noise density for this should be 40 nV/√Hz. If I understand this correctly, then white noise on a scope with a 100 MHz bandwidth shouldn't be larger than 0.4 mV peak to peak. However, when I use the product, matching the conditions on the datasheet as well as I can, I see noise which is an order of magnitude larger. So, I'd like to know some more details about how you did this measurement and how I could remeasure that 40 nV/√Hz number here in the lab. In particular I'd like to know what device you used to measure and its input impedance, or what resistance you measured across if you did that. The support team suggested I should ask here since they were unable to answer this question.
Thanks!