This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2901: pull-up voltage

Part Number: LP2901


I'm using the LP2901 because I have many signals that I need to ensure voltage levels aren't erroneously too high.  So the high input voltage range of the LP2901 works well.  However I'm taking the outputs of the LP2901 to AND gate IC's with a supply voltage of 9V.  I've used the LP2901 in other designs and always use a pull-up R on the outputs, but it's always been to Vdd.  For ease of not having to put a ton of voltage divider R's in the design can I pull up the outputs of the LP2901 to 9V rather than my Vdd of 28V?