Other Parts Discussed in Thread: INA226,
Dear Sirs,
This is Quanta PEE in taiwan than Ask the following questions.
1.
We should use shun model. There are 16bits in total, we can set it through I2C.
1bit=+-2.5uV, 16bits=81.9mV. This represents the cross-voltage that can be detected = +-2.5uV to +-81.9mV.
Is my understanding correct?
2.
What is the default value of reverse current (cross voltage)? ?mV, ?bits.
3.
Does the voltage detect to protect the reverse current through I2C? Can we set bits through our MCU? or it need Burning tool?
Thank you very much