Part Number: THS4211
Hello,
I want to operate the THS4211 on VCC=+7V and VEE=_-5V.
Is it OK?.
Giora
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Giora,
The THS4211 can operate with a VCC of +7V and a VEE of -5V. I have attached a snippet from the THS4211 recommended operation conditions for operating with dual supply or single supply. The recommend max difference in the voltage supply is 15V and recommend min difference in the voltage supply is 5V. You would have a difference of 12V. To ensure maximum output voltage swing, I would recommend biasing the input signal and amplifier to midsupply which in your case would be 1V.
Thank you,
Sima