This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4277: opa4277 analog

Part Number: OPA4277
Other Parts Discussed in Thread: OPA4196

Dear Sir, please answer

I need to pick up a replacement of OP747AR amplifier.  The case may be different, it is important that the parameters are close.

Important:  power supply +/- 15 V, rail-to-rail output, short sircuit current 30 mA, output are stable with cap load of over 500 pF,  frequency range 1 kHz.

Circuit application, please see in attach.

TIA

Sincerely,

Vladimir Naumenkov

8015.Circuit 3.docx0871.OP747.pdf