This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4196: OPA4196 & booster

Part Number: OPA4196
Other Parts Discussed in Thread: TINA-TI, OPA2990, TLE2071, TLE2141

Dear Michael, dear Thomas, thank you. 

Please, answer

I will use amplifier for the next purpose: I need to generate positive and negative pulses 5...14 V amplitude, 10....50 millisecons duration. 

1) Probably, you mean a distortion of the "step" type at the moment the voltage passes through zero? Please see figure 1 in attach.

Amplifier's harmonic distortion is not so important in my application.  The capacitance at the output of the amplifier, most likely, will not exceed 5nF.

2) Based on this, can I apply my circuit without any modifications? Please, see attach.  Will I need a compensation to assure stability?

3) Does it make sense to install a 100 ohm resistor between the output of the amplifier and the bases of transistors T1 and T2 ?

TIA

Sincerely,

Vladimir Naumenkov

2860.Figure 1.docxOPA196 boost_3.TSC