Part Number: THS4042
Other Parts Discussed in Thread: OPA211, OPA1611, THS4031, THS3121, THS3111, THS4032, OPA564
Hello guys,
One of my customers is concidering using THS4042 to drive 0.1uF output capacitor and 2kohm output resistor with gain 1.
They have a few questions as the follows.
Q1. In case of 0.1uF output capacitor driving with gain 1, can Figure 68. Noninverting, Unity Gain Schematic on page 17 in the device datasheet be used?
Q2. When Figure 68 schematic can be used, .Is 20ohm resistor not needed betwee THS4042 output and 0.1uF capacitor like Figure 65. Driving a Capacitive Load for Extra Stability on page16?
Q3. Do you have any other op amp which can drive 0.1uF output capacitor and 2kohm output resistor with gain 1?
The customer operation conditions: VCC=+/-15V, Gain=1, Vin(pp)=100mV, CL=0.1uF, RL=2kohm.
Your reply would be much appreciated.
Best regards,
Kazuya.