This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4196: OPA4196 & booster_3

Part Number: OPA4196
Other Parts Discussed in Thread: OPA196

Dear Michael, good day!

Thank you

Excuse me, I have not clearly understand about additional resistor 10 k. 

You wrote:  "2. Can it be set to a zero output current mode - no, it can't - at minimum provide a pulldown R to the negative supply to shift the operation towards an NPN on bias. then, say you desired a true 0V output, then say a 10kohm to the negative supply keeps the NPN on closing the feedback loop."

Please, see attach, I understand correct connection of resistors R3 and R8 ?

Sincerely,

Vladimir Naumenkov

5001.vladimir_OPA196__work2.TSC