Part Number: TLV3701-Q1
Other Parts Discussed in Thread: TLV7031, TLV7011, TLV7032, TLV1805-Q1
Hi Staff,
Let me ask a question in TLV3701-Q1
The signal also rises at the same time as the Vcc power supply rises (0 → 3.3V).
※IN+(0→1.8V), IN-(0→2.45V)
As a result, 3.3V High-Level is output to the OUT pin at the same time as the power is turned on and the signal is applied.
High-Level is output and transitions to Low-Level after about 2.5ms.
* There is no load connection.
* Since IN+ < IN-, I was expecting Out=Low, but I would like to know the reason why High is output for 2.5ms.
Question
1.If the power is turned on and a signal is applied at the same time, will the Out pin be output for about 2.5ms?
2.Is there anything wrong with starting up the power and applying the signal at the same time?
best regards
cafain