Other Parts Discussed in Thread: OPA2192
Hello,
I have some questions regarding OPA2140 used to
- buffer a 5V precision voltage reference to increase the load current
- invert the same 5V precision voltage reference to create a -5V reference output (using opa2140 in inverting amplifier classic configuration)
The opa2140 is power supplied in +/-12V (thus +/-5V is far from saturation limits)
First question :
- what is the minimum load current gauranteed for all temperature at opa2140 ?
figure 31 is only typical, as well as short circuit current in page 7
Second question :
Apart external resistors tolerances (in inverting amplifier configuration, and voltage reference own tolerance), what are the parameters to be considered for the operational amplifier OPA2140 when defining the worst case output voltage tolerance (considered are new buffered precision reference voltages) ?
Thank you for your support
Best regards.