Other Parts Discussed in Thread: AMC1200, ISO224
Hello,
I will use AMC1200Q1 to supply proper voltage to ADC of TI 320F2837D DSP. First , I measure the 110V rms voltage using LEM LV25-P, then I will connect AMC1200Q1 to output of the voltage sensor.
I am a little concerned of the pin connection of AMC1200Q1. How can I connect the voltage sensor to opamp ? Are there any resistors and capacitors should be connected between opamp and voltage sensor ?
I check the datasheet but it is a little complicated for me.
Input of the DSP board can accept the voltage range between 0 and 5 volts.
Output of the LEM voltage sensor is in the range of between 0 and 3 volts.