This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA381: opa381

Part Number: OPA381
Other Parts Discussed in Thread: OPA2381, OPA380

At your opa381 datasheet, p.7 are shown square response 200 kHz. Scale shown is 100 ns/div. This is uncorrect. Change to 500 ns/div for 3 pictures, please. Vladimir

  • Hi Vladimir,

    I think this is no mistake but intentional. The transient response of one half wave of a 1MHz square wave with Cf=3pF is shown. So, the 100ns/div scaling is correct. Additionally, the pulse response with Cf=16pF is shown. As the settling time of OPA381 is too long for a 1MHz square wave, a 200kHz square wave is used which - after having changed its time scale for reasons of simplicity - is overlayed on the original curve .

    Kai

  • Hi, Kai. see p,8 of OPA80, please. Transient curves for 380 & 381 look similar at equal speed: 100ns/div. Slew rates of 380 & 381 are differ by more than 6 times: 80 & 12 v/us. It is this contradiction that has caused my doubts. (I already used OPA2381 for Large Area photodiode and now I`m looking faster TI OA).

    Vladimir

  • OPA380, certainly....

  • Hi Vladimir,

    Thanks for your post. Please accept delayed response as many of us are on holiday break. We will support you shortly.

    -Tamara

  • On that web page, under parametric table, the Vos of the OPA380 is given as 25mV which is incorrect. It's 0.025mV.
    Do as you will with this info.

  • You are correct.  There is a typo in parametric search of OPA380 Vos showing 25mV instead of 25uV.

  • Happy New year, Kai!

    Of course, 25mV vs 0.025mV is typo. But my comment was about something else.
    I would like to return to the original message (Dec 23, 2019 1:22 PM).
    There is a contradiction in the documentation for two similar TIOA: OPA380 & OPA381.
    Compare “Large-Signal Step Response” (1v/div) at p.8 (OPA380 datasheet) & p.7 (OPA381).
    For OPA380 circuit feedback RC= 10kohm * 2,5 pF = 25 ns or t (0,1) = 55 ns. This corresponds to the speed 100 ns/div.
    For OPA381 circuit two feedback RC1= 50kohm * 3 pF = 150 ns & RC2= 50kohm * 16 pF = 800 ns are shown. Time scale is the same (100 ns/div) and transients are finished by 50 and 200 ns. Too fast for RC 150 & 800 ns. This is incorrect. Everything will return to normal if scale will be changed to 1us/div for OPA381 datasheet. Similar changes should be made for Small-Signal Step Response figures close at hand.

    Vladimir

  • I had written my comments for guru kai klaas69.

  • Vladimir,

    You are correct that OPA381 datasheet large-signal horizontal scale should be in 1us/div instead of 100ns/div.  This can be easily seen by measuring the slew rate in the graph below, which would result in ~120V/us instead of 12V/us - changing the scale to 1us results in correct slew rate: SR=4V/300ns=~12V/us 

    A small-signal rise time is a function of the effective bandwidth, fc - see below: tr=0.35/fc

    If you calculate the expected rise-time for Rf=50k and Cf=3pF, you obtain tr=0.35/(2*Pi*RC)=330ns while for 50k and 16pF the rise-time is ~2us - thus, as you correctly pointed out, the scale in the graph below should be 1us/div instead of 100ns.  I will inform the system engineering team of the errors.  Thank you.

  • Marek Lis, thank you for attention. My next layout will be done using OPA380 binding N-JFET BF862.

    Vladimir

     P.S. this year there is no snow in Moscow at all.

  • Hi Vladimir,

    Thank you for your inputs. Just so you know, we are working on the new precision TIA with integrated switches - see below. 

    P.S. We can send you some snow from Arizona... :)

  • Hi Marek, snow in Arizona is as rare as Moscow without snow (it did fall tonight)...

    Very interesting, I would like to work with your new TIOA. If possible, please send samples. A similar amplifier with switches and output buffers ADA4350 recently released Analog Devices.

    Vladimir.