Other Parts Discussed in Thread: OPA991
Hi sir,
Please kindly recommend TI P-P solution to replace NCS21911 SOT-5P.
Other spec requirement is:
Offset: 25uV-800uV
VCC: +36V (at least >16V)
Thanks a lot!
BR,
Sean Liao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sean,
Is the offset voltage range for the room temperature? If so then OPA990 in SOT-23 package will be P-P compatible with NCS21011 SOT package. This will be 1 MHz part. https://www.ti.com/product/OPA990/samplebuy
If the offset voltage is an absolute max (across temp) then OPA991 will fit the bill. http://www.ti.com/product/OPA2991 This will a 4.5 MHz part. The dual-core version of this part is already RTMed. Single-core is in the development phase. can you give me the detail on the end equipment and when will the customer be going to production?
Regards,
Sanjeev