This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DIP-ADAPTER-EVM: Schematics available?

Genius 11945 points
Part Number: DIP-ADAPTER-EVM

Hello Team,

it may sound trivial but can you share the schematics or layout, please? How are e.g. the SOT23-5 pins connected to the DIP-8 pins? 1->1, 2->2, 3->3, 4->4, 5->5 or 1->1, 2->2, 3->3, 4->6, 5->8?

Thanks and Best Regards,

Hans

  • Hans,

    Adapter connection between SOT-23-5 and DIP-8 (or SO-8) must be made according the pin functionality - see below.

    Therefore,

    SOT23-5        DIP-8 (SO-8)

      pins 1      ->        pin 6

      pins 2      ->        pin 4

      pins 3      ->        pin 3

      pins 4      ->        pin 2

      pins 5      ->        pin 7

  • Hi Marek,

    it looks like there has been a change, please see photo below.

    Best Regards,

    Hans