Hi, staff
Please ask questions using the waveforms on page 9 of the OPA567 data sheet (SBOS287A).
Q1.
The lower left waveform “ENABLE 10Ω Load” has a ± pulse output.
After ENABLE transitions from Low to High,
the output has a +1V pulse about 1us later and a -1.5V pulse about 7us later.
Why is such a pulse output?
Q2.
The output of the bottom left waveform "ENABLE 10Ω Load" is valid for 8us after the rising of ENABLE,
but the input vs. output delay is unknown because the input waveform diagram is not published.
I think there is no delay because it is analog.
Q3.
The lower right waveform “ENABLE 1Ω Load” has ± pulses output.
Why does the pulse amplitude after ENABLE decrease when the output addition is small?
Q4.
What countermeasures are required to prevent pulses on the output?
best regards
cafainOPA567 Out-pulse.pdf