Other Parts Discussed in Thread: LMV321, LMV321A
I am using the LM321 as a front end to DAC on my MCU. I am looking for gain of 1 [ Vout = Vinput * (1+R31/R30) ]. My R31 is 0 ohms, R30 is not installed. Gain should equal 1. So what is in on + should equal that on the output. Or I thought: I have produced 10 of these boards as a prototype and found that 5 of the boards deliver 5V on the op-amp output with the input of 5V. (perfect)!!! However, the other half are consistent on producing maximum of 4.5V on the output (pin 4). Both boards behave the same when the input voltage < 4.5V. So my question is what is causing this and how do I fix this?
I have played with my R31 & R30. Added 0 ohm & 1K resistor on R30 with no difference. I don't want to have to adjust the gain because in production, I need consistent behavior and cannot afford to tune each of the boards. Am I doing something wrong with my design or do I have a bad batch of Op-Amps?