In the process of using ina260, reading the current and voltage values of the path will result in a probabilistic data exception, with a value of 0 or much greater than the normal value. The measurement of IIC signal quality is OK. Is there any other reason that may cause this abnormal phenomenon? The data of abnormal voltage is read as the value of current. Is the data string wrong? Here are the ina260 related circuits and IIC signal waveforms
Ina260 design schematic diagram:
IIC signal waveform of CPU end:
Read path voltage data:
Read path current data: