This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV772: There are some error on datasheet(Rev.F) of lmv772

Part Number: LMV772

Hi, 

 I think there are some error on the datasheet lmv772. I download datasheet of lmv772 with a version  "SNOSA04F –MAY 2004–REVISED SEPTEMBER 2010 "

And I find maybe there are some errors:

Page 16:

Page 19:

  • Hi  John,

    Question 1 on p.16. 

    You are correct. It should be R2 in fo = 1/(12*pi*R2C). Reasons are:

    At DC and low frequency, Vout/Vin = -R2/R1. 

    When R2 and Xc's impedance are equal, the gain is starting to decrease at -3dB point, which it generates the pole. R2 = 1/sC or fp = 1/(2*pi*R2*C).

    Question 2 on p.19. 

    You are also correct. R1 and R4 should have been switched, see the image below. You can solve the bottom circuit by applying superposition method. 

    Thanks for pointing out the mistakes. I will make a note of it. 

    Best,

    Raymond