Other Parts Discussed in Thread: LM7705
Hello,
I'm trying to simulate an INA333 circuit in TINA and it does not appear to be working.
My input sine wave is set a min/max of 0 - 13mV. The gain should be approx 92 according to the datasheet, per my gain resistor of 1.1k. As seen in the screenshot below, the output is not as expected (should be a sine wave with min/max 0 - 1.96V offset by 200mV.
What am I doing wrong?
Thanks!