Hi team,
customer use INA219 measure current, find the have 50~60 mA current error.
test condition as below:
1. bus voltage is 12V; current is 1A; Rshunt =1mA set Curretn _LSB =1mA, reg05=0x1000, reg00 is default.
read current register data and get the current is 1.045A.
2. Change current from 500mA to 2A, always have 50mA gap with actural current.
the quesitons is:
1. does this is normal for INA219 current accuracy?
2. how to redruce the measurement gap.
thanks.