This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA377-Q1: Some questions about using OPA377 to build a current limiting circuit

Part Number: OPA377-Q1
Other Parts Discussed in Thread: OPA377

I use the OPA377 as  a current limiting circuit.

The voltage of the 3 pin of OPA377 is 0.19V,but  the voltage of the 4 pin of OPA377 is 0.72V。

The voltage of the 3 pin and the 4 pin should be equal is 0.19V.

The voltage between the 2 pins of the connector P3 also should be 0.19V,but it is 0.72V。

What is the problem?

thanks!