This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA326: Negative current issue with TINA & INA326

Part Number: INA326
Other Parts Discussed in Thread: INA826

Dear,

I'm trying to simulate with TINA FIGURE 16. Programmable ±5mA Current Source. of INA326 datasheet

Recreating the file

INA326_jp.TSC

It simulates well +5mA to 0mA , but the curve is flattedned to 200uA from 2.5 to 5V ... MAybe an issue with the INA326 model ?

How can I simulate  to obtain -5mA ?

thanks in advance