This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR111-2EVM: 0.5 to 4.5 volt input and 4 to 20 mA output verification and confirmation needed

Part Number: XTR111-2EVM
Other Parts Discussed in Thread: XTR111

Dear Sir,
I wanted to use your XTR111 current converter IC to get 4 to 20mA output
with an input of 0.5 to 4.5 volts

Based on the data sheet and XTR111 evlauation user maual I have arrived
at the following values for the input circuit

R10 = 1k, R8=10k, R6=115k, VREG= 5Volts, input VIN will be 0.5 to 4.5 volts
RSET = 2.25k,
Output will be 4 to 20mA for the given input 0.5 to 4.5 volts

would you kindly help me verify the results and confirm, if there is any
deviation or correction needed please let me know

(for your information I have calculated based on the data given and did
not do any practical experiments with the evaluation card since I do not
have the same)

attached a screen shot of the schematic given the user guide for your ready reference

with best regards

K. Ganapathy
9395331274
kgp@spm.co.in
SPM Instrument India Pvt Ltd
Hydreabad India XTR111 user guide evaluation card.pdf