Hi,
In fact, I have read about Automotive shunt-based isolated current sensor reference design ( http://www.ti.com/lit/ug/tiduel5/tiduel5.pdf?ts=1588591688374) in the section 2.4.2 that this 50-mV device is amplified at a gain factor of 41, which results in output voltage levels of -2.05 V to +2.05 V on the differential output stage of an isolated amplifier. This means that it amounts to a peak-to-peak voltage of 4.10 V on the output terminals of the AMC1302-Q1, but when we open the datasheet of the AMC1302-Q1 we see in figure 26 that the differential output is approximately 2.05V when the differential input is 50mV. My question is why did they say that the output terminal peak to peak is 4.10V when it should be 2.05 V based on the figure that I joined and thank you in advance.