Part Number: OPA2365
Hi guys, I'm analyzing how much current the OPA2365 consume. Supposing I don´t know what is the value of the load at the output, what values should I choose from the datasheet to get an estimated consumed current value?
For example in pg 6. There appear a IQ (Quiescent Current Per Amplifier) of max 5 mA which is the consumed with IO = 0 A. But at the other hand, I think it is needed to have into account the current provided to outputs; so in pg 5, section Output, appears a value ISC (Short Circuit Current) of max 65 mA (which is the only value I see related for current of outputs). So can I say that one amplifier of this chip would demand a current max around IQ + ISC = 5 mA + 65 mA = 70 mA?